OPTIMIZE INSULATION PERFORMANCE WITHOUT COMPROMISING PROFITABILITY

Reduce costs and better insulate with Solstice® Liquid Blowing Agent (LBA), pure or in blends with hydrocarbons vs Vacuum Insulated Panels (VIPs)

Contact Us

Are you paying more for insulation performance than you really need? 

As energy efficiency regulations evolve, refrigerator manufacturers need innovative ways to meet new requirements – all while maintaining profit margins and attractive retail price points for consumers. With Honeywell Solstice® Liquid Blowing Agent (LBA), pure or in blends with hydrocarbons, you can optimize insulation performance without compromising on profitability or retail pricing.

Increase Performance And Increase Margins

As the industry standard, Solstice® LBA minimizes the need to use more expensive Vacuum Insulated Panels (VIPs) while realizing a 10% improvement in insulation performance vs hydrocarbons. By replacing 1 sq. meter of VIPs using our high-performance Solstice® LBA in your blends, you could save between $5-$10 per refrigerator.

Learn more

New Energy Labeling Requirements by Region

Understand what energy consumption requirements for refrigerators are affecting your region

Comparison of maximum energy use requirements for refrigerator-freezers (25°C)

Source: Lawrence Berkeley National Laboratory [LBNL] analysis

Accelerating The Global Adoption Of Climate‑Friendly And Energy‑Efficient Refrigerators (Page 8)

Notes:

  1. For refrigerator-freezers, energy consumption at 25°C according to standards in Colombia, Panama, El Salvador, Costa Rica, India, Mexico, Singapore, and the U.S. is assumed to be less by 25 per cent than the energy consumption at 32°C. Energy consumption at 32°C according to the EU standard is assumed to be greater by 25 per cent than the energy consumption at 25°C. South Africa’s requirement is equivalent to the current EU B class.
  2. The maximum energy use requirement for India, U.S./Mexico, and other countries are for frost-free type, refrigerator-freezers—automatic defrost with top-mounted freezer without an automatic icemaker, and refrigerator-freezers, respectively, as defined in the standards.
  3. The comparison is based on calculations for a two-door frost-free refrigerator-freezer with 300 L storage volume and freezer compartment accounting for 30 per cent of total volume

Solstice® LBA offers an ultra-low global warming potential (GWP) of one, and is an alternative to HCFCs, HFCs, and hydrocarbons (cyclopentane). When used alone or as a blend with cyclopentane, Solstice® LBA can provide better insulation performance than using cyclopentane and vacuum insulated panels (VIPs).

Blends of Solstice LBA / Cyclopentane

K-Factor Of Refrigerator Foam

EE Test Result For Refrigerator

Energy consumption vs. Blowing agent

The appliance industry is facing an environmental challenge resulting from the use of high GWP materials, such as hydrofluorocarbons (HFCs), hydrochlorofluorocarbons (HCFCs), or less energy efficient materials like hydrocarbons, commonly used as blowing agents in the production of insulation foam.

Honeywell has invested more than one billion dollars in its Solstice® technology, having anticipated the need for lower global-warming-potential (LGWP) solutions more than a decade ago. Today, Honeywell is helping customers lower their greenhouse gas emissions and improve energy efficiency without sacrificing performance.

  • Based on hydrofluoro-olefin (HFO) technology, Solstice® LBA has a global warming potential (GWP) of 1, 99.9% lower than HFC blowing agents.
  • Solstice® LBA helps customers realize energy efficiency goals, with a 10% improvement in insulation performance vs hydrocarbons.
  • Solstice® LBA is non-ozone-depleting, nonflammable (ASTM E-681 and EU A11), listed under the U.S. EPA’s Significant New Alternatives Policy (SNAP) program to replace ozone-depleting substances, listed on the TSCA inventory/registered under REACH, VOC-exempt (per U.S. EPA), and manufactured in the U.S.

Solstice® materials eliminate millions of metric tons of CO₂ equivalent every year. 

Technical Documents

Case Studies

Honeywell Solstice® LBA Adopted By Al-Essa Of Saudi Arabia For Their Energy Efficient Freezers
Read More
Achieving Gains in Thermal Performance Thanks to Insulation System Developed by BASF using Honeywell’s Solstice® LBA
Read More
A Commitment to Sustainability and R&D Lead to Breakthrough Solution for Midea
Read More
Solstice® LBA Helps Festivo Achieve Energy Ratings and Environmental Targets
Read More

The Blowing Agent Alternative Enabling Key Improvements in the Household Appliance Industry

In response to increasing environmental regulations, evolving energy efficiency requirements and focus on higher insulation performance with a lower cost, the fourth-generation hydrofluoroolefin, Honeywell’s Solstice® Liquid Blowing Agent (LBA) is the environmentally-preferred alternative for original equipment manufacturers.

Contact Us

Do you need a cost-effective insulation method to improve energy consumption of residential refrigerators? We’re here to help you achieve compliance with new energy efficiency (EE) labelling regulations. Contact us to learn how.

Mezclas Solstice LBA para electrodomésticos